This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25882默认输出电压异常

这是我的设计原理图,焊接了两块板子,两种状况。目前没有接锂电池,图中VBUS=5V,1.8V_IO没接,I2C没控制,默认情况下:

板1: SYS=4.4V左右,BAT电压为0V,TS=3.7V

板2,SYS=7.2V左右,BAT电压为0V,TS=4.2V

x 出现错误。请重试或与管理员联系。