4串锂电池16.6V,要求充电器电压24V 11A,充电电流10A(由于用电源模拟充电器,电源最大输出5A,因此先设定充电电流为4A),预充电流为1A,插上充电器,指示灯表明正在充电,可充电电流为0,测过个引脚,都满足充电条件,请问一下还有哪些地方需要注意
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
4串锂电池16.6V,要求充电器电压24V 11A,充电电流10A(由于用电源模拟充电器,电源最大输出5A,因此先设定充电电流为4A),预充电流为1A,插上充电器,指示灯表明正在充电,可充电电流为0,测过个引脚,都满足充电条件,请问一下还有哪些地方需要注意