This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8863 VDD電壓問題




目前我在使用LP8863的時候,有遇到一些問題點,因此需要評估相關的風險性與影響程度

目前的線路架構是沒有使用chargepump,但VDD目前是接到3.3V.

後來在文件說明上看到須將VDD接到5V.  但因修改不易,需要下一版本才能改接到5V.

因此我需要了解當VDD接3.3V的影響程度,與產品應用的風險性有多大..