This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求750V输入 110V输出3kw 隔离DC/DC技术方案或参考设计



我需要设计一个电源模块,主要指标如下:
标称输入电压: DC750V
输入电压范围:DC675V~DC825V
控制电压范围:DC77V~DC137.5V
输入过压保护:DC900V~DC930V
输入欠压保护:DC600V~DC570V
输出电压:DC109V
输出过压保护:125V+3V
稳压精度:1±1%
输出纹波电压:<500mV
额定输出电流:30A
稳流精度:1±1%
输出限流值:≤1.1In
输出电压调整率:±1%
额定负载效率:≥90%
过温保护:≥95℃
均流不平衡度:≤5%
额定负载温升:≤40K
使用温度:允许在-40℃~70℃环境中使用,短时10min 内允许85℃环境温度下使用。
风扇散热

请帮忙推荐成熟的设计方案或参考设计