This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62090 VS TPS62090QRGTRQ1



1. 温度项为何差异这么大?请说明原因?

2.TPS62090RGTR为何热阻会增大?芯片材料有变化吗?

  TPS62090RGTR TPS62090QRGTRQ1
温度  -40 to 85  -40 to 125
V(ESD)
Human body model (HBM)
±2000V ±2500
V(ESD)
Charged device model (CDM)
±500V ±1500
RθJA
(Junction-to-ambient thermal resistance)
47°C/W 45.6°C/W
RθJCtop
(Junction-to-case (top) thermal resistance)
60°C/W 58.9°C/W
RθJB
(Junction-to-board thermal resistance)
20°C/W 19°C/W
ψJT
(Junction-to-top characterization parameter)
1.5°C/W 1.1°C/W
ψJB
( Junction-to-board characterization parameter)
20°C/W 19°C/W
RθJCbot
( Junction-to-case (bottom) thermal resistance) 
5.3°C/W 4°C/W