This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3478 BOOST升压 3.6V输入 36V输出 300mA负载 加载输出电压不正常 空载输出电压正常

Other Parts Discussed in Thread: LM3478

LM3478   3.6V输入 36V输出 300mA负载  加载输出电压不正常  空载输出电压正常

输出电容为300uF。

空载时候输出电压为36V

加载120R电阻  输出电压只有11V左右   

调节电感大小(3.3uH 5.6uH  10uH)输出电压还是11V

调节频率(500KHZ   1MHZ )输出电压还是11V

下面是 空载时候测量的。输出电压是36V。

CH1通道 黄色波形是MOS管栅极波形     CH2通道蓝色是开关节点的波形

(通过这个波形可以看出电感充电完成后,MOS管断开后,开关节点上脉冲电压达到35V,经过二极管整流后输出电压能够达到36V)

下面是300mA 120R负载波形,输出电压只有11V

CH1通道 黄色波形是MOS管栅极波形     CH2通道蓝色是开关节点的波形

(通过这个波形可以看出  电感充电完成后,MOS管断开后,开关节点上脉冲电压只有12V,此时栅极驱动电压占空比已经非常大了,而且栅极波形非常稳定,频率在500KHZ)

想不明白电感上脉冲电压为什么只有12V, 而且脉冲电压上不去?输出电压所以只有11V左右。输出电容是300uF。