This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq40z50-r1 RSOC=0时对应的电池电压



4串电池组,在做RA阻抗的Learning Cycle时,放电至12V停止也学习成功了,生产量产srec文件,写入到新板中,校准后去做充放电验证,发现RSOC=0时,电池组电压在13V左右,而在Gas Gauging的设置也是12V截止,如下,这是什么原因导致呢?

"Gas Gauging","IT Cfg","Term Voltage","12000","mV"
"Gas Gauging","IT Cfg","Term V Hold Time","1","s"
"Gas Gauging","IT Cfg","Term Voltage Delta","300","mV"
"Gas Gauging","IT Cfg","Term Min Cell V","2800","mV"

  • 补充:
    验证过程:2A充电到taper电流,2A放电到12V(但是RSOC=0时电压13V左右),2A补充电到出货电压
  • 您确认一下RSOC为0时,是不是其中一串电压低于Term Min Cell V,这样就会强制terminate。

  • 各电芯的电压很平衡

  • 学习的时候,SOC是在什么电压报0%的?
  • 刚查了update status由06更新至0e的LOG记录,RSOC=0时,电压是在12.42V左右

    做ra learning的步骤如下(4串4.2V电池组),此时导出a.srec,en使用,reset

    1、放电至11.8V/410mA;2、搁置5H;3、16.8V/2A充至41mA;4、搁置2H;5、820mA放电至11.8V;6、搁置5H,做到这里时,update status=06,各ra_flag均为0055,按文件接着做,7、16.8V/2A充至41mA;8、搁置2H;9、820mA放电至11.8V;10、搁置5H,做到这里时,update status=0e,各ra_flag均为0055

    导出B.srec、A.gg,并修改cycle count=0、qmax cycle count=0、update status=02存为b.gg,在新板写入a.srec,写入b.gg,新板、新电池组做老化学习

    问题

    1、在做老化学习时,由于update status=06,是不是要做充饱搁置,放完搁置,才能更新update status为0e?搁置至少要多长时间?(有做了个成功,是按learning的搁置去做的)

    2、如何确保放电至Term Voltage=12V时,对应的RSOC=0?

    Term Voltage 12000
    Term V Hold Time 1
    Term Voltage Delta 300
    Term Min Cell V 2800