This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教TPS40422使用PMP6924原理图做1.0V 50A输出,一上功率就输入短路

Other Parts Discussed in Thread: TPS40057

我完全使用pmp6924方案做的1.0V的电源DCDC,输入12V,带XILINX FPGA,上电后电压正常,一旦加载运算(功率会上升到输出1V 21A,输入大概应该2A多点点)的时候就是导致输入电源短路(实验了两种电源,一个是5A的 atten实验电源,电流到头一旦加载运算会电流保护,fpga重启。第二个是12V 7.7A的明纬开关电源,也是相同的情况)其他不变,使用之前tps40057制作的电源没有这个问题,外部电容基本上是按照6924做的,应该从哪里下手解决呢?