我使用TPS65910AA1给AM3359供电,为什么板子的PMIC VRTC输出电压都是2.2-2.4V,并不是标称的1.8V。是芯片的问题吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问 你的VRTC和AM335X是如何连接的?
如果你把AM335X 复位信号拉低,让主芯片不工作,是否还有同样的问题?
测量下VRTC上电波形,是否有变化?
现在我这边使用TPS65910A31A1 搭配AM3354使用,上电后tps65910 VRTC输出为2.2V,我们做了如下的试验:
1) 断开两个芯片的VRTC线路,输出1.8V
2) 把RTC_RST信号拉低,使处理器不工作,输出1.8V
3) 断开RTC线路,使用VDIG1给处理器的VRTC供电,电源芯片的PWREN脚直接短接到电源芯片的VRTC输出,这时候VRTC输出1.8,VDIG1输出1.8
4) 使用示波器测试VRTC波形,发现刚上电时VRTC输出时1.8V,大约15ms后,电压升高到2.2V
5) 目前板子上发现VRTC电源在走线时,从引脚出来有一段线很细(4mil),长度大约90mil
6) 在VRTC线路上增加假负载,1.2K负载时电压为1.96V,1K时为1.55V
是否能把你的VRTC部分的原理图截图上来?
另外:目前板子上发现VRTC电源在走线时,从引脚出来有一段线很细(4mil),长度大约90mil-----为什么要这么做?
Hi,Jerry
我参照TMDSSK3358_3H0009_REV1_2B_SCH_ALLEG16_2这个电路图设计了一个开发板,使用的AM3352+TPS65910A3A1RSL,但通5v电源后电源管理IC没有电压输出,是需要先配置电源管理IC吗,电源部分我是按照参考电路原原本本做的。
你好
我的也是使用的AM3352+TPS65910A3A1RSL,但通5v电源后电源管理IC没有电压输出,测试VRTC发现只有1V左右,你的发现问题在哪了没