Other Parts Discussed in Thread: TPS61165, TPS61169
我用12V供电,九个led串联,并联三串;输出标称值为27V,360mA,输出功耗在11.7W;
第二款屏输出标称值为27.9V,240mA,输出功耗在8W左右;
请问TPS61165这款芯片支持吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
0.96A是最小峰值电流限制,可以理解。0.95*1.2这个最大电流是按照经验来计算的对吧,至少需要1.2倍容量