我用TPS54231的电源方案得到了12V——>+5V的转换,但是我不知道怎么测量电源的效率,专家能否介绍几种方法?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
该电源的输入电压应该有个范围,输出电流应该有个额定值。
比如输入电压范围为8-14V,输出电流额定值为5A。
你可以选择多个功率点进行测量,
比如8V输入,输出电流按10%递增至额定值(即0.5A,1A,1.5A,2A,2.5A,3A,3.5A,4A,4.5A,5A)。依次测量
效率。可在一定情况下超过额定输出电流值测量效率。
将输出电压分别换成10V,12V,14V,重复以上测量。
在同一坐标系中,做出不同输入电压情况下,效率按输出电流变化的曲线。