This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678电源管理芯片UCD9222有关问题

Other Parts Discussed in Thread: UCD9222

       您好!我们设计了基于C6678的电路板,在调试过程中,遇到了有关UCD9222芯片配置的问题。
       我们的电路板和开发板设计一致,除了系统供电从开发板的12V改为了6V。在使用GPIO-TO-USB下载线连接FUSION digital power designer 工具对UCD9222配置的过程中,始终没有VOUT和POWER GOOD信号输出。我们使用开发板配套的ucd9222的xml文件进行配置,并根据我们的实际情况调整了输入电压的配置,现在可以在监控界面中看到 VIN是正常的6V,但仍然没有0.9V和1V的输出电压。
       以上是我们在工程中遇到的问题,希望可以得到TI技术支持的帮助,万分感谢!