1. 支持双输入VIN充电
2. VIN充电电压范围>12V
3. 充电电流>1.5A
4. 电池电压VBAT默认4.35V,支持可设定
5. 支持PCB通孔板设计(例如>0.65mm pitch,或者类似QFN封装)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. 支持双输入VIN充电
2. VIN充电电压范围>12V
3. 充电电流>1.5A
4. 电池电压VBAT默认4.35V,支持可设定
5. 支持PCB通孔板设计(例如>0.65mm pitch,或者类似QFN封装)
Hi
2560x只有一个VIN输入口,有没有支持两个输入Port的IC,也就是USB和12V DC adapter可以同时插入此IC?
好的,不过bq2416x系列最高VIN电压只支持10.5V,如果需要插12V adapter可能没法用。