请专家帮忙推荐一个24V转±15V/±2A的 DC/DC电源芯片。谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好:
1、负电压输出,网络好像不能做仿真。不知道输出电流能否可以达到2A,能否请你们TI工程师帮忙做个仿真。
2、两个TPS54360并联起来用同一个24V输入,会不会有地电平问题?
1.关于仿真可以参考附件,用Tina即可
2.你负压-15V,加上输入24V,只要Vin DC大于39V就可以7823.TPS62150 Inverter.TSC