This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ucd9222通过I2C配置问题

Other Parts Discussed in Thread: UCD9222

各位好,我在配置UCD9222芯片时遇到了问题,具体如下:

我通过Fusion软件生成I2C脚本,并把CPU的I2C与UCD9222的PMBUS连接(此时PMBUS_CNTRL)脚接上拉,然后通过I2C方式把此脚本中的数据依次写入UCD9222芯片中,I2C可以正常写入,但配置完成后,UCD9222 DPWM输出1.8V左右的固定电压,请问这是什么原因呢?

由于项目很急,麻烦各位多多指点,非常感谢!