This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92513电感选型

各位,我在使用这款buck芯片时,发现参考选型计算出来的RT引脚接200k电阻开关频率576k,根据这个计算出来的电感值在22uH。然而这款芯片PWM调光只支持100~1000Hz,调光时就发现电感有啸声。这个电感值应该是不够的了,请问调光电感值是不是不能这么选了。

另外,输出的波形是正常的方波,并无问题。有个很奇怪的现象就是,我想让脉宽渐变,实现光照强度缓慢变化,即占空比从0加到50%,然后50%到0循环,频率1k。结果很快输出就关断了,BOOT电容上面只有1.9V,不知道是什么原因。

看来可能需要用IADJ模拟调光了。