This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC3843的电流采样脚的RC参数对环路稳定性的影响该如何分析?

Other Parts Discussed in Thread: UC3843

各位前辈:

我仿照UC3843的参考电路做了一个反激电源。原理框图类似如下:

我实际电路图中,Rcsf=1k,Ccsf取330uF~1000uF。我发现电源在Ccsf取1000uF时,出现自激振荡。输出纹波从30mV提高到90mV,振荡频率约为30kH左右。当Ccsf取330uF,电源正常,纹波30mV,频率400kHz。开关频率为400kHz。

我看了一下手册对Rcsf、Ccsf的取值说明。如下图:

我看手册只是从RC滤波的角度出发,说RC的时间常数要大于开关周期。从这一点来说,Ccsf取330pF~1000pF应该都是满足条件的。应为开关频率fs=400kHz,开关周期Ts=2.5us。Rcsf=1k,Ccsf=1000pF,RC时间常数t=RcsfCcsf=1us;Rcsf=1k,Ccsf=330pF,RC时间常数t=RcsfCcsf=0.33us;都是比开关周期T小的。

可是为什么Ccsf取大一点会引起自激呢?

我怀疑是不是Rcsf、Ccsf其实是在电流内环中,会影响到电流内环的性能?可是我又不知道该如何定量计算这个Rcsf、Ccsf的参数。手册中对环路补偿参数的分析与计算也只是对谐波补偿和基于运放的补偿参数,并没有对Rcsf、Ccsf的参数计算,或者说认为Rcsf、Ccsf并不在环路补偿内。可是,实际中Ccsf的取值确实影响着稳定性。在我做的反激电源中,Ccsf取300pF电源稳定,Ccsf取1000pF电源不稳定,请问这该如何分析呢?除了RC时间常数小于开关周期这一条,还有其他限制来用于Rcsf、Ccsf的参数设计吗?需要考虑电流内环吗?电流内环该如何分析计算呢?感觉很复杂的样子。手册中的算例似乎也没有考虑电流内环补偿参数的设计?