This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq25703调试问题 REG0x0B/0A寄存器参数设置不成功、拉低适配器电压



1.  5V2A适配器给2cell串联8.4V电池充电;设置所有寄存器参数并读取时;发现只有 InputVoltage Register  REG0x0B/0A寄存器参数仍然为0,和设置不一致;其他参数都可以正常读取到;请问大佬们是哪里配置需要更改;

2.使用5V2A适配器可以正常充电1.7A左右(输入电流REG0x0F/0E为2A);更换为5V1A充电器发现适配器电压直接被拉低到3.7V左右;只有更改输入电流REG0x0F/0E为1A才不会出现拉低;但是IC如何根据适配器进行 输入电流REG0x0F/0E进行调整还是有其他设置要求?

3.因此怀疑拉低5V1A适配器电压参数和 InputVoltage Register  REG0x0B/0A寄存器有关;但是一直写入不成功,请问有大佬知道吗?

  • 1. InputVoltage Register REG0x0B/0A假设所使用的适配器提供了一个恒定的电压,预计用户根本不需要修改这个寄存器
    2. 关于电流限制您参考数据手册8.3.7 Two-Level Adapter Current Limit (Peak Power Mode)
  • 您好,了解并验证了电流限制您参考数据手册8.3.7 Two-Level Adapter Current Limit (Peak Power Mode)是针对于峰值功率模式的的毫秒级设置;设置参数后并没有起到相应的作用;目前遇到的问题是输入电流设置2A情况下;5V1A充电器会出现拉低充电电压即VBUS到3.7V左右;开机后亮灭屏充电;无法兼容两种适配器长时间在正常电流下充电;