我有一个灯板,输入电压为8-45V,接12个3W的灯,有没有什么稳定的方案?急
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
12个3W的LED,串联或并联都可以,单颗LED是3.2v 1A左右电路,不需要隔离,
如果你的输入电压是在8~45V动态变化,建议你采用单串连接(Vout 大约38V)。由于输出电压介于输入电压范围内,所以需要采用Bulk-boost拓扑结构。请参考LM3421的AN-2010。修改少部份参数就可以满足你的需求。
Johnsin Tao给我推荐的事TSP40210这颗芯片,具体哪一颗稳定性和性价比一些?另外,论坛里面有谁用这个芯片画过板啊?
还有一个问题,我这边输入的是3跟线,一根是电源负极,另外两根是电源正极,电压是一样,都是12V或者是24V.导通的时候两组电源正极永远只有其中一组有电压输入(相当于汽车的远近光灯,近光暗,远光亮一些),但要在同一片板上实现这两组输入的时候其中某一组有输入的时候LED亮度有差别,一组亮度高,一组亮度低,亮度相差20%左右。
这两颗芯片谁能实现呢?
Hi
TPS40210还提供了一个汽车LED灯的方案: http://www.ti.com.cn/tool/cn/pmp5713 (动力应用,您需要用到汽车级别的芯片TPS40210-Q)
这个方案的输入电压是5.5V~18V,输出12V/1A, 所以您还可以模仿这个设计,关于不同的输入电压,会有不同的亮度,您可以参照这个设计采用不同的PWM调光占空比去控制或者其他的方式都是可以的。(但是这个方案您要注意,当您的输入电压是40V时,LED的电压达到38.4V, 也就是实际升到的电压将是78.4V)
实际上就您目前的应用而言,因为是3根线,如果12V,和24V都是恒定有电的话,您可以只用12V这组电压,然后用TPS40210,设计成为boost架构,参照datasheet第二十四页的方案更加简单。
有谁用过TPS40210?我的要求能不能实现,特急啊,一个星期一眨眼就过去了,还一点眉目都没有