This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ucc3895电压控制模式、低电压空载输出时OUTC/OUTD占空比在46%-54%变化



200Khz移相位全桥,电压模式,体内运放做跟随, 采用碳化硅全桥整流,有假负载3K3w,输出电压15V-100V

闭环调试时发现,在低电压空载输出时,变压器原边有占空比丢失现象(而且是一个固定的方向),查出是OUTC和OUTD占空比在抖动(46%-53%),且OUTC占空比抖动相对严重,但OUTA和OUTB占空比几乎没有抖动(示波器同步观察下,前后波形重合)。

然后开环调试时,发现给定值(20PIN)0.9V时,OUTC和OUTD的占空比抖动现象一样。(均未有过流保护现象,环路在过补偿下依然存在)

查看了TI的技术支持文件说,只有峰值电流模式才会出现该现象(OUTC/OUTD占空比抖动),而我用的是电压模式,希望帮帮忙,比心。