This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50R1电池学习放电过程中RDIS置位是怎么回事?



电池包在放电过程中,电量大概放置10% 左右的时候,RDIS置位了?这是怎么回事? 静置无小时之后,又消除了。学习的过程我是按照给的操作步骤来做的,配置好之后先reset,然后放空至3V左右,静置五小时候,再打开gauge_En 进行充电吗,充电至FC置位,静置了大于2小时之后,有进行放电吗,结果在放电的过程中就出现了RDIS置位的情况。

请问这大概是什么原因导致的呢? 我该怎么做呢?

谢谢

  • The Ra update is disabled if any of the following conditions are met. The GaugingStatus()[R_DIS] is set to indicate the Ra update is disabled.
    During the optimization cycle, the Ra update is disabled until QMax is updated (that is, Ra will not be updated if Update Status = 4), OR
    • Ra update is disabled if the charge accumulation error > 2% of Design Capacity, OR
    • During a discharge, a bad Ra value is calculated:
    – A negative Ra is calculated or
    – A bad RaScale value is calculated.
    A valid OCV reading during RELAX mode or a fast Qmax update without an OCV read will clear the [R_DIS] flag.
    您在跑learning之前,是否完成配置参数,选择chem ID,校正等步骤。
  • 是的,我在学习之前完成了参数配置,化学ID选择,校准这些步骤。然后reset进行放电至3V左右,静置五小时之后,再Guage_EN进行充电至FC置位,再静置大于两小时的时间再进行放电,放电大概在10%左右的时候RDIS置位了,放电结束后大概4小时左右RDIS又取消了。Ra_flag就一直是0555,就是QMAX没有更新,updata status也一直就是06,更新不到0e。

    还有就是我导入配置参数之后学习之前导出的备用SREC文件,提醒我导入成功,结果data memory里的数据就没有更新,cycle count没更新,Ra_flag也没,没有更新。不知道这是怎么回事。

    请帮忙解答。

    谢谢!

  • 你好,我也遇到类似问题,请问您现在解决了吗???
    请问是配置好之后先reset,然后放空至3V左右,静置五小时候,再打开gauge_En 进行充电吗?我现在是看手册说配置好之后先打开gauge_En,然后reset,然后放空至3V左右,静置五小时候,再进行充电,之后充完电静置2h,updata status就没有变化???