This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63700问题

Other Parts Discussed in Thread: TPS63700

 请教诸位,我们用的模拟板使用了TPS63700,  转换5V to -12V。使用电路基本与DS里推荐的一样,除了分压电阻,推荐是121K和1.2M,我们使用150K和1.5M。

    TPS63700负载为,一片TPS7A3001将-12V转为-10V给3片运放供电。

    问题如下;(模拟板独立工作,之间没有任何关系),电源板输出5V/6A。

           设备(背插式)插一块电源板和一块模拟板,一切OK。测量COMP管脚为0-0.6V左右。

           设备(背插式)插一块电源板和二块模拟板,一切OK。测量COMP管脚为0-0.6V左右。

           设备(背插式)插一块电源板和三块模拟板,TPS63700无法正常工作。测量COMP管脚为2.7V左右,将该管脚与GND短路,TPS63700正常工作了。

           如果把负载TPS7A3001去除,插三块板TPS63700也正常。

           如果设备插入其他5V的负载的板卡,对模拟板的TPS63700有时也不能工作。

           两个电源的EN脚都是默认接VIN。

           TI有没有COMP内部的电路图,我们想更改一下连接COMP管脚的电容再进一步测试。