Other Parts Discussed in Thread: BQ40Z80
我们在使用BQ40Z80进行6-7串BMS设计,严格按照文档要求进行老化学习,但是电量准确度老化学习一直不能成功老化至1%,只能老化至3%,看到Qmax更新,也观察到Ra表在更新。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: BQ40Z80
我们在使用BQ40Z80进行6-7串BMS设计,严格按照文档要求进行老化学习,但是电量准确度老化学习一直不能成功老化至1%,只能老化至3%,看到Qmax更新,也观察到Ra表在更新。
我是严格按照该文档要求进行老化学习的:
1. 使用29.4V,10A的恒流恒压模式将电池充满,截止电流1A;
2. 静置2小时;
3. 使用10A恒流放电模式对电池放电,截止电压19.5V;(因为老化设备最高支持电流为10A,所以没有按0.2C(12A)的倍率进行老化,但文档说明0.1C-0.2C的放电倍率学习是被允许的)
4. 静置5小时;
5. 循环1-4步骤3次以上;
电芯使用松下NCR18650BD, CHEM_ID=2072, 7S20P,25.2V/60AH;
BQ40Z80配置参数:TERM V=19.6V,TERM I=0.6A,由于容量较大,实际容量及电流均按5倍进行衰减,即实际截止电流=3A;