This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50电量计算

Other Parts Discussed in Thread: BQ40Z50

BQ40Z50作为TI的高度集成的电量计,使用起来很方便,但是有很多原理都是一知半解的,如下有些问题,希望TI大神们能帮忙解决:

1.电量计是否是采集每一串的电压,然后根据每串的电压(这里不知道是根据每一串电压还是总电压),然后结合ID(根据放电曲线,RC和电压的关系),就可以计算出电池组在这个时候的Remain CAP,进而根据更新的FCC去计算RSOC?

2.导入量产文件的电量计,如果通过上位机发送Reset,是否要进行重新学习?Reset之后,QMaxPassedQ会清零。

3.如果导入量产文件IT使能不关闭,经过循环测试(测试条件可能达不到学习条件,例如静置时间30分钟),这样电量计是一直处于学习的状态,那这样是否学习可能会失败,如果在测试过程中关闭IT使能,出货再打开,那这样客户使用的条件就更达不到学习条件(他们也会做各种测试)

4.QMAX更新时间,看手册上说是,充电结束后会更新,但是我做出来的是放电结束更新,然后静置一段时间也更新了,请问这样有问题吗?

  • 1, The chem id is a look up table which the gauge uses for determination of state of charge during
    initialization. The gauge also uses this table as part of the IT algorithm to predict remaining capacity.
    2. 不需要在重新学习。
    3, 您出货之前已经学习过了,出货之前IT enable是为了客户使用过程中更新IT的参数延长电芯使用寿命。
    4, 这个是正常的