This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教BQ27545、BQ27546 校准电流 如何计算!

ccOffset ,boardOffset  根据读 0X79 读到的数据再根据以下运算。

int ccOffset = (((uint16_t) block[8] << 8) + (uint16_t) block[9]);
signed char boardOffset = block[10];

float ccGain = (float) (校准值/ (float) ((int) 平均值- ((ccOffset + boardOffset) / 16)));

按这个计算无法校准电流,数据是100%写进去了。为什么 floating2Byte 也是根据官网的例子转换的 ,但是Battery Management Studio得到的值跟我自己计算的不一致,例如:我计算得到的ccGain的值是 5.13,通过官网文档提供的计算方法 floating2Byte(ccGain)后,得到rawData[0]  is 80、rawData[1] is a1 、rawData[2] is 47、rawData[3] is b0,然后写进数据区后,Battery Management Studio得到的值偏差很大,这是什么原因呢?求解答!qq632845069。