This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2776输出异常

Other Parts Discussed in Thread: LM2776

我这边使用LM2776的时候,遇到一个问题:

电路拓扑如下:

现象描述:

1. 电路上电,LM2776输出端测试为0.7V左右的正电压,断开LM2776负载,LM2776可以正常启动,启动后在接入负载,输出正常。测试断开后的负载端,显示仍有0.7V左右的正电压,怀疑此正电压可能是从运放正电源串过去,LM2776未启动之前,输出端有正电压造成其无法启动。

2. 测试-5V的负载电流,总共约80mA,LM2776的输出能力手册显示为最大200mA。

 

3. 目前解决办法:在LM2776输出和负载中间加了MOS管电路,即保证了当LM2776启动后有一定负压时,才能使MOS管导通,这样隔离了负载端串过来的正电压,可以正常启动。

 

问题:

1. 想请教下LM2776 驱动双电源运放时,是否可以直接作为负电压供电芯片?

2. 如果双电源运放,当只接入正电压,而负电源端无输入时,是否会存在负端会感应过去正电压?

2. LM2776 用上述的mos隔离电路,是否可行?是否存在隐患?

4. 是否有好的负压方案推荐:主要用途是为25个四运放提供负电压,负载约为80mA。

x 出现错误。请重试或与管理员联系。