Other Parts Discussed in Thread: BQ24725
3节18650电池,在配置充电IC过程中,充电电压配置为13V,直流电源供电为13.5V,输入电流配置为4A,设置充电电流为1A时,实际充电电流只有700mA ;设置充电电流为1.256mA时,充电电流为910mA;设置充电电流为2A时则无法充电,为什么充电电流与配置的充电电流值不一致?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: BQ24725
3节18650电池,在配置充电IC过程中,充电电压配置为13V,直流电源供电为13.5V,输入电流配置为4A,设置充电电流为1A时,实际充电电流只有700mA ;设置充电电流为1.256mA时,充电电流为910mA;设置充电电流为2A时则无法充电,为什么充电电流与配置的充电电流值不一致?
在CV mode设置充电电流,充电电流不会变。
您根据下面的方法再试一下。
set VBUS = 20 V, ICHG = 1.536 A, and VREG = 8.4 V,increased VBAT in CV mode until IBAT tapered down to 200 mA。the ICHG register setting to 1.024 A, but IBAT stayed constant at 200 mA.