This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24133 DC 电压输入,第二个MOS管不导通什么问题

当我插上电源DC座的12V电源后,BQ24133的输入端第二个MOS管不导通,前面第一个导通,请问是什么引起,不管接不接电池,三节电池,VREF电压3.3V正常

  • Q2是 reverse blocking FET.
    您可以按照数据手册9.3.9 Enable and Disable Charging一节内容逐项测一下,看是否某些条件不满足导致无法充电。
  • 我在电路中,在电池放电的MOS管我接错了是N沟道的,我现在等P沟道MOS管到来,请问我在没有更换这个MOS管之前,8脚ACDRV是17.8V,只有一个最前面的MOS管导通,第二个MOS管不导通,是这个电池放电的MOS管引起的吗
  • 在上图中,我的电池放电的MOS管,现在使用了N沟道的,在P沟道MOS管没有索样到来之前,Q2107的这MOS管不导通,Q2106是导通的,R2437电阻端,2个MOS管的删极是17.8V,为什么只有前端的MOS管导通,后面的MOS管不导通,尝试,将Q2108MOS管去掉不焊接,也是Q2107不导通,搞不明白了,我直接外接3.3V到2个MOS管的删极是可以2管导通的