您好:
1、我使用54386给FGPA供电,输出3.3和1.2v,目前调试中发现FB1和FB2上的电压只有0.4v左右,但是手册中说明是在0.8v,请问什么可以导致该问题。
2、Functional Block Diagram图中SW引脚有很多相连的点,请问这个点是什么关系 ‘与或非’?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好:
1、我使用54386给FGPA供电,输出3.3和1.2v,目前调试中发现FB1和FB2上的电压只有0.4v左右,但是手册中说明是在0.8v,请问什么可以导致该问题。
2、Functional Block Diagram图中SW引脚有很多相连的点,请问这个点是什么关系 ‘与或非’?
正常输出3.3V的匹配电阻是4.7k和1.5k。测出FB引脚0.45V,输出的电压降低到1.8v。同样另外一路正常输出1.2V的网络也降低,电阻是1k和2k,FB 0,23V 输出0.69V。请问这个问题可能是怎样导致的,由于输出电压低,导致FB低;还是FB低导致输出电压异常。
电路应该没有正常工作,你1.8V输出的SW节点波形和这个一样么?应该不一样吧
检查下3.3V这一路焊接有没有问题,另外你的原理图和PCB也传上来看一下吧