Other Parts Discussed in Thread: TPS61221, TPS61220
你好!我使用的TPS61221在VIN变化时,VOUT随着变化,如VIN=4.2V时VOUT=3.98V,这是啥原因?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
TPS61221是固定3.3V输出的升压芯片,并且不具备LDO功能,也就是说输入电压必须小于3.3V输入,输出才能有正常的3.3V稳压输出,请试验用1.5V输出看3.3V输出是否正常?
当输入电压高出3.3V时,占空比为0,升压功能不在存在,输入电压会通过二极管(以及MOS)直接流向输出,而已输入电压和输出电压的关系将是相差Vd(二极管管压降,忽略电压压降)
Hi
如果你的设计目的是超过3.3V的输出,并且是需要升压, 你可以选择TPS61220,但是这个芯片的最高输出电压只有5.5V,你需要注意。或者你需要选择其他的芯片,请明确你的选型要求:输入电压范围,输出电压,以及最大负载。
我最近用这个芯片也出现这个问题了,在0.1-3.3V时,能稳定到2.8V左右,不是3.3V,我用的电感是10UH的(因为公司现在没有4.7的),请问这个是不是电感影响的啊
建议关注两个地方: 1. EN引脚。注意要满足使能的条件:当输入低于1.5V时,最小是要达到0.8Vin;当输入大于1.5V时,EN最小值是1.2V。 请实测确认下。 2. 输出反馈的FB,重点读一下datasheet的P13,有提到一些设计参考,比如FB典型值值500mV,R2小于500KΩ等。需要遵循。
你好:
我最近遇到和您一样的问题,我的电感是4.7uh,不过输出也是2.7V至2.8V。同样的电路,之前还是好好的。请问您是怎么解决的?
你好:
我最近遇到和您一样的问题,我的电感是4.7uh,不过输出也是2.7V至2.8V。同样的电路,之前还是好好的。请问您是怎么解决的?