Other Parts Discussed in Thread: TPS54361, TLV62130
看了一下tps54361的数据手册,发现EN默认是上拉使能的,现在想用三片TPS54361级联,并按照一定的上点顺序启动,前一级的PWGOOD(开漏输出)去使能后一级的EN,现在EN默认上拉就是上电就启动了,那我是不是要把它下拉到地,但是PWGOOD又是开漏输出,这样电路怎么设计呢? 谢谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
想再请教一个问题,TPS54361内部EN那里是一个1uA的电流源,默认状态下是上拉,我现在用FPGA的IO口(3.3V CMOS电平)直接接在EN引脚上,外部不用任何上下拉电阻,想让上电时芯片处于关断状态。但是FPGA上电配置有一定的时间,在此期间IO处于未配置状态,那此时芯片是打开还是关断状态呢?
另外那个电流源上拉怎么理解呢,之前的芯片(TLV62130都是内部电阻上拉),谢谢回复