This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1充电电流ChargeCurrent()和什么参数有关?如何设置最大充电电流?

Other Parts Discussed in Thread: BQ34Z100, BQ34Z100-G1

ChargeCurrent(): 0x32/0x33 只读寄存器输出可充电电流,这个参数应该和Design Capacity参数有关

比如我将Design Capacity设置为22000,Charge Current Tx-Ty设置为100%

达到这个温度条件后ChargeCurrent()值为22000mA

请问可以在不改变Design Capacity值的情况下,使充电电流变大吗?