Other Parts Discussed in Thread: LM5117
想请教一下各位大佬,我用ti的WEBENCH Designer设计了一个lm5117的电路,设计参数输入44到46v,输出36v,输出电流3A,然后测试的时候发现输出电压太低,只有两伏左右,调大下端分压电阻过程中fb管脚上升到0.65V后不再上升;
测量管脚过程中还发现,供电电压在15v以下时vcc管脚电压为7.6v,但UVLO管脚电压低于1.25V;在调大vin电压的过程中,UVLO电压上升但是vcc电压下降,UVLO和vcc电压始终无法同时满足正常工作要求;
测量HO输出波形发现有设计的248kHz频率,但是是占空比极低的尖峰脉冲,而且持续约一百多个周期后就会出现一段几伏的直流电压;
在对照着芯片手册检查电路时发现说Ramp对地的电容应不超过2nF,我用的是10nF的,换成0.47nF后上电测试,空载,电源电流0.04A,芯片发热,是不是烧了啊?还有之前这种情况是什么问题呢?