This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于BQ25700A 电池拔出后,CELL_BATPRESZ为0,是否还有最小电压输出

根据SPEC引入: NVDC-1 配置可将系统电压稳定在电池电压范围内, 但不会低于系统最小电压。即便在电池完全放电或被取 出时,系统也仍会继续工作。当负载功率超过输入源额 定值时,电池会进入补电模式并防止系统崩溃。在这里提到电池拔出,由于·电池拔出导致CELL_BATPRESZ为0,此时还能保证有最小电压输出吗?这里最小电压输出应该是不做电池拔出检测吧

  • CELL_BATPRESZ pin is pulled below VCELL_BATPRESZ_FALL to indicate battery removal. The device exits LEARN mode, and disables charge. REG0x15()goes back to default.
    上述描述中说明CELL_BATPRESZ为0,默认电池拔出,此时REG0x14 为0,即没有充电电流,充电电压回复默认值,这个取决于您的cell设置。
    When BATFET is removed, the system node VSYS is shorted to SRP.详细请参考数据手册53页8.6.5.1 System Voltage Regulation
  • 感谢您的回复,我的意思是电池拔出,因为MCU检测拔出后会控制场效应管得状态让CELL_BATPRESZ 为0,而不是BATFET REMOVED。此时系统没电了,与数据手册第1页:“NVDC-1 配置可将系统电压稳定在电池电压范围内,但不会低于系统最小电压。即便在电池完全放电或被取出时,系统也仍会继续工作。”矛盾
  • 您说的是对的,仔细看了一下是我理解错了,问题解决