This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用 BQ25703和bq40z50-r1来进行充放电管理,发现相同代码,有时候可以充电,有时候不可以充电

Other Parts Discussed in Thread: BQ40Z50-R1, BQ25730, BQSTUDIO

各位好:

我目前使用BQ25703和bq40z50-r1来进行充放电管理,通过bq40z50-r1的寄存器0x14和0x15来获取电池需要当充电电流,使用获取的值来配置bq25703,

同时根据输入的电压和电流来配置bq25703输入电压电流,根据系统工作电压配置bq25730来配置最小系统电压

根据上述配置,相同代码有时候可以充电,有时候不可以充电,充电时bq40z50-r1寄存器0x16为0x84(可以正常冲对岸充电),该充电但没充时,该寄存器为 0xc4.

4表示访问被拒绝.

烦请各位大神帮忙指教,非常感感谢