This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28180电感电流波形畸变的问题。

之前看到过类似的帖子,TI的员工回复是因为芯片电流采样饱和造成的。我看了28180的datasheet,有一些疑问。关于采样电流饱和,也就是说,ISENSE引脚的电压过高,如果触发SOC保护,按照datasheet的说法,是通过一个接地电阻给Vcomp电容放电,以减小PWM占空比。占空比减小,电流应该降低。为什么从波形上来看,电流反而升高了呢?

畸变电流波形就是这种情况,电路只有中间部分冒尖。

另外一个疑问就是关于ICOMP引脚的。datasheet说,这个引脚电压低于0.2V就会禁用控制器。这个引脚的电压不是应该是跟随平均电感电流的么?那么在电流最小值的地方,ICOMP引脚电压应该会低于0.2V,这时候控制器就被禁用了么?

  • HI
    升压电感饱和吧?
  • 我是根据你们的360W的EVM功率慢慢加上来的,开始在600W输出的时候,出现这个问题,我也以为是电感饱和,但是我换了更大的电感,这个尖峰电流依然存在。后来我把电流采样电阻调小,尖峰就消失了。从最开始的0.032的电阻,调整到了现在0.015。现在在220V输入,1150W的输出时,再次出现了这个问题。但我用电流探头检测到的电流实际上只有12A左右,而根据SOC保护计算出来的电流保护值应该有17A。