Other Parts Discussed in Thread: TPS40057
在使用TPS40057时遇到的问题描述如下:
负载在全负荷工作时,负载电流为40A。产品在进行低温测试时,发现在-30℃时,通电不能启动。于是做了如下排查测试:
1,常温下,用电子负载单独测试电源5V输出,输入端加24V电源,30A负载带载启动,能正常启动。
2,-30℃时,用电子负载30A带载启动,无法启动,输出电压为0,分别尝试20A,10A,5A带载启动,都无法启动,2A可以启动。然后逐渐增大负载电流,都可以启动(怀疑是通电之后电源板温度上升,电源周围温度上升后,恢复正常)。把Q1的c和e短接,再进行低温测试,30A负载能正常启动。
3,常温下测试Q1带负载能力,负载为60mA时,输出端(发射极)电压由17.7V跌落至8.5V。通过调整三极管基极电阻,R6=1K,R18=4.7K,以增大Q1的负载能力,调整之后,负载为130mA时,Q1输出电压由18.1V跌落至8.3V,再进行低温测试,仍然无法正常启动。
4,为了进一步提升Q1的负载能力,把Q1更换为达林顿三极管,实际测试Q1负载能力,此时在1.5A负载时,电压由17.3V跌落至15.6V,负载能力已经大幅度提升,在进行低温测试。仍不能正常启动,和2中现象一致。
5,把E7-E10四个1000uF电容去掉,再装上一颗470uF电容,进行低温测试,带载启动电流能提升到5A,30A仍不能带载启动。
最后我们测试把过流检测电阻改为使用1M后低温下可以运行了,请教下560K(设定的电流大于40A)这种情况下为什么10A就异常么?是影响到期间内部哪里了产生这种情况了么