This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

电路级联,TPS61222 tlv61225

Other Parts Discussed in Thread: TPS61222

如图,将300KHZ,1V的正弦信号输入到整流升压电路

经过整流升压后得到输出为

但是将整流滤波电路和升压电路级联,发现升压芯片的输入只有600mV,输出为1.65V

经测试,整流模块 和 升压模块单独工作时都正常,但是级联在一起后,TPS61222 的输入电压明显下降,从2.3V变为600mV,不满足其正常输入。

问题:

1 这种现象的原因是什么呢,与阻抗匹配有关吗?

2 在两个模块之间加了一级电压跟随器,发现当不级联TPS61222时,仍正常工作,级联后电压跟随器波形变为不规则三角波,且幅值仅有400mV

3  这种现象一般有什么解决办法?