This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62240DRV 的输出电压问题

规格书中写到:, R2 should be 180 kΩ or 360 kΩ. The sum of R1 and R2 should not exceed approximately 1 MΩ;这样一来,R2最小值是180KΩ,R2最大值就是820KΩ,按照计算公式Vout=Vref(1+R2/R1),最大的输出也就只有3.3V左右。我问下R2真的只能配置成180K或者360K这两个值吗,那要是我要输出Vout=4V的怎么办?