This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28950EVM的疑问



请问,UCC28950EVM中R8,R9;这两个功率电阻的作用是什么?谢谢

  • 和C1,R6组成吸收电路。

  • D4,D6,R6,C1,R8,R9共同构成了吸收电路,原理是当PSFB从续流阶段到传输能量这两个状态切换时,副边同步整流管Q5,Q6中有一个的DS电压会上升到2*Vp/Nps,但是由于副边漏感的存在,使得DS电压存在振荡,存在尖峰,高于了2*Vp/Nps。为了保护同步整流管,需要对DS上的电压尖峰进行吸收。

    而加R8,R9的目的是为了将谐振尖峰能量的一部分传递给负载,这样不至于将能量白白浪费。

    R8,R9的另一个作用是在上电时,有一个通路:T2副边-D4(D6)-R8//R9给输出电容充电,可以使得输出电压迅速建立。

    吸收电路的设计要保证C1上电压的最小值高于2*Vp/Nps,根据漏感大小,以及开关周期设计RC。

    建议你可以观察的:

    (1)用探头同时看看D4的阳极、阴极电压;

    (2)将R8,R9去掉,但是必须给C1并一个或两个小阻值的功率电阻,观察C1上电压,上电时输出电压建立过程以及效率(不过这里效率的改善是很小的)。

    希望这些建议能有所帮助,有什么结果可以一块讨论。

    • UCC28950EVM中
    • T3和T4的具体参数是多少??同名端是哪些脚,T3和T4的具体制作参数在哪里能下载到???

    • UCC28950EVM中
    • T3和T4的具体参数是多少??同名端是哪些脚,T3和T4的具体制作参数在哪里能下载到???
    • T2的具体制作参数在哪里能下载到???
    • 总不能为了自制变压器实验把原板上的给拆开吧???