This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8860 BOOST 不起振的问题



相同的外围硬件设计,有些板卡可以起振,但上电就输出900mA 的总电流,有些板卡上的来LP8860,不起振。完全是按照规格书中输出电压40V的参考设计来的,求解答,以下是原理图,其中前置MOS及sense电阻已拿掉,后边NC的R63 贴的0 ohm电阻。情况是,将驱动代码烧录后,有一个板卡可以点亮一个背光但是电流很小。在通过code改变电流时,开始改电流一个小时内时OK的,后来直接输出900mA总电流,后来这个板子就挂了,在测试其他的板卡Boost一直不起振。

  • HI
    将电路传上来看一下啊和规格说明一下。
    不过你提到有的有问题,是否大部分没有问题,如果是这样,建议你优先检查一下焊接,特别是不起振的板子
  • 如果负载阻值过大;没有达到额定输出电流,系统就是全开放状态,输出逻辑“1”而没有脉冲。因此;是否有脉冲,并不是判断依据。建议测下;是否能稳流。

    另外;无图无真相。无图无回答。