Other Parts Discussed in Thread: TLC5954
TI工程师:
您好!最近有个LED驱动项目要用到LED驱动芯片,最后打算用TLC5954,有一下两个问题
1,sclk频率问题,手册上写的SCLK频率是30MHz最大,最小是空,高电平和低电平时间最小是10ns最大是空,我不是太明白手册的意思是频率最大不能超过30MHz,高低电平时间只要大于10ns就可以?我用的是50MHz的GPIO口。手册5页
2,手册上推荐的连接方式为DIN串联,LAT,SCLK,BLANK共用,我是用5个TLC5954如果按照手册的方式连接,我要给第五个写数据,我是不是要写五次数据,才能把第五个数据写进第五个芯片里?如果我要读第一个SID数据,是不是要写五次空数据才能从第五个芯片的SID脚输出第一个芯片的SID数据?手册33页
以上两个问题我理解的是否正确,如果不正确,第一个问题50MHz的GPIO口能否满足,第二个问题五个TLC5954怎么连接。
谢谢!