TPS63020电路在老化的时候出现L1对地短路
电路图如下:
输入电压:5V;输出3.3V@300mA 为节能采用对外脉冲式输出:输出电压波形如下
正常使用的时候,设备电路正常,一旦加入高温箱后,温度大于50℃以后,出现随机短路现象。单独使用电池供电没问题,一旦使用老化车供电,多台设备一起连接在一起,就会随机出现芯片L1对地短路现象,请帮我分析一下原因,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.