This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24725A电池充放电控制

Other Parts Discussed in Thread: BQ24725A

硬件描述:按照BQ24752A手册P36页参考电路,设计了输入电压5V,单节电池充放电控制电路,mos管选用参考电路型号,ACDET设计为2.6V大于阈值电压2.4V,VCC管脚通过4.7R电阻进行供电保护,I2C总线上拉至1.8V,与CPU接口电压保持一致。

出现问题:未接入电池情况下,初次上电,CPU未对I2C进行配置,BQ24725A的ACDET管脚2.58V,REGN输出为低,ACFET RBFET两个输入保护MOS管G极输出为低,后端供电母线输出不正常(正常情况下应该接近适配器输入电压5V)。

请各位大神解惑,BQ24725A为什么输出不对。