This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5155设计问题

Other Parts Discussed in Thread: LM5155

使用LM5155做一个升压模块,输入3V,输出15V。希望在启动以后使用输出作为LM5155的供电。

手册里面介绍了两种方法:1、将输出接入BIAS,使用内部稳压模块,此时VCC大概6.8V;2、将输出接入VCC,但要求Vbias≥Vcc,或者加二极管防止反向。

问题:能不能将BIAS直接不接,输出连接VCC。说明文档里面只是说BIAS是给VCC的稳压模块供电的,没有提到别的用处。

请专家指教,谢谢!

  • Hi
    芯片要首先启动采用输出,所以BIAS电压必须是要有的。等有了输出,将输出给到VCC这样是可以的。
  • 谢谢专家!如果BIAS不接:

    假设芯片没有启动,此时输出电压应该是输入电压-二极管压降,将此电压接入VCC,如果启动不了,我们考虑可以接入一个高电压至输出和VCC,例如6-12V,手动启动,这样是否可行?如果输入电压足够高,芯片启动,那就没问题了,BIAS可以甩空。

    以上理解对吗?