我装上新的bq20z45芯片,读出的数据都是1717,需要哪些步奏来初始化。
还是我新买的芯片有问题?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,可以尝试一下一下步骤
1.到http://www.ti.com/tool/bq20z45evm-001下载BQ20Z45-R1 bqEASY Software 安装
然后在EVSW软件里找到一下界面,先试一下3的按键能否使之正常工作,不行就按照图中的步骤,重新下载senc文件,附件后缀名为txt 改为senc就可以使用了,看看这个步骤能够解决您的问题。谢谢!
编程电压可以在EVSW里找到这个参数,默认的是7500mV 。谢谢
[Power(Power)] Flash Update OK Voltage = 7500