This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC5320驱动输出打嗝问题



我使用UCC5320SCEVM评估板驱动一块SiC-MOSFET,电路图如下。其中R3,R2换为0Ohm,C16去除,IC芯片加装散热片和风扇。

Vcc1 5V, Vcc2 20V, 驱动信号5V,占空比50%

当工作频率上升到2MHz时,输出波形出现间歇性打嗝,(见下图,蓝色是Vcc1,粉色是驱动信号,绿色是输出)

输入端Vcc1和输出端Vcc2电压波形平稳,并没有触发UVLO的迹象。芯片表面温度大约为90度左右。

将Vcc2降到15V后,此时波形正常。将工作频率上升到3MHz,此时温度又达到90度左右,再次出现了打嗝现象。

 

有趣的是,继续增加信号频率后,打嗝频率也会随之增加(但宽度不变,在2ms左右),温度保持在90度左右不变,就好像是“过热保护”功能一样。

芯片的资料上并没有介绍有关于过热保护的信息,因此想咨询一下发生这种现象的原因,希望得到工程师的回答,谢谢大家。