This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

两个TPS543C20并联输出80A电流PCB设计

Other Parts Discussed in Thread: TPS543C20

设计使用两个TPS543C20并联(12V~0.9V)输出80A电流,请教PCB设计时,电感输出端外接一大块铜皮,需要在该铜皮上打过孔连接到内部电源层,通过电源层给其他器件供电。请教各位在该铜皮上打过孔(过孔能通过80A电流),需要打多少过孔?(假如铜皮为0.5oz,过孔内径10mil/外径22mil)

  • 这么大电流,只有0.5oz也是没啥了。建议5oz。
    过孔电流密度按30A每平毫米电流密度计算即可。
  • 目前是这样的情况,PCB板卡已经设计完毕,产品正在调试,出了一些问题。整个PCB设计为12层,该电源输出0.9V在top、bottom均有一块约18mmx18mm铜皮(再次确认该铜皮为0.333oz,不是0.5oz,不好意思),在内层有一个0.9V电源层平面,该平面铜皮1oz。设计0.9V可以输出80A,目前PCB该电源铜皮上有101个过孔(内径10mil/外径22mil),现在想知道这些过孔能否过80A电流,或者说这些过孔最大能通过多大电流?请教!!!!!

  • 请教一下,1)建议5oz是指单个top层设置为5oz吗?2)“过孔电流密度按30A每平毫米电流密度计算”这个能给介绍一下怎么计算吗?请教一下!!!!

  • Hi
    铜皮为0.333oz肯定是小了,这么大电流。
x 出现错误。请重试或与管理员联系。