This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54331中12V转3.3V电路中的一些问题

这是TI官网的设计电路图,我焊接完成电路之后,测得的电压是4.5V左右,其中我最后的两个100uf的电容没有焊上,会对电压产生如此大的影响。

  • 哦。。。如果告诉你;你那4.5V也是不靠谱的值,不知是何感想。呵呵!

    没装电容如同削掉手足,看你咋蹦达。。。呵呵呵

  • 电容也要看是什么电容的,有的可以省略,有的不可以,你这个电路图是webench生成的吗,电容放在分压电路后面,看上去不是很重要。可是你看官方数据手册的电路,这两个电容是和D1、L1构成一个回路的,相当之重要,手册上9.2.2.6是专门讲这个电容的取值的。你把他们看成一个整体,就感觉到相当之重要了。

  • Hi
    输出稳压电容必须要的,整个转换需要到输出电容储能稳压。