如下图原理图:
此电路现采用9V做输入电压(不用之前的12V),±13.5V给运放一个OPA2171供电(负载电流不超过100mA),实际5001输出电压是+13.88V和-12.88V。并且随着负载运放数量增多,负电压幅值还会继续降低。请教一下此电路中元器件参数如何做修改才能保证负电压稳定在-13.8V这样。或者电路上需要做什么调整?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如下图原理图:
此电路现采用9V做输入电压(不用之前的12V),±13.5V给运放一个OPA2171供电(负载电流不超过100mA),实际5001输出电压是+13.88V和-12.88V。并且随着负载运放数量增多,负电压幅值还会继续降低。请教一下此电路中元器件参数如何做修改才能保证负电压稳定在-13.8V这样。或者电路上需要做什么调整?
Hi
电路图没有上传上来?
负压也是变压器隔离出来的吗? 一般这种情况会与变压器设计有关,具体要看电路图。